VIA RAID Tool Component
                    for Windows XP Embedded SP2
                           9/22/2005
           Copyright (C) 2002-2005 VIA Technologies, INC.

1. Release note
   This package is ver 1.0, adapted from VIA RAID Tool
   RaidTool_V552 for the VIA SATA/IDE RAID controller
   such as VT6410, VT6420, VT6421, VT8237 and VT8251.

   VIA RAID Tool implements main RAID functions (like RAID 0) 
   in conjunction with the hardware, hence it's very easy for you 
   to achieve RAID functions using VIA RAID Tool.

   VIA provides the user with this sample component implementation,
   to ease development and test effort. The user, however,
   is advised to obtain the latest available driver and author
   his or her own components.

2. File description
   This package contains 8 files as described below.
                                 
                                       Readme.txt       this file
09/21/2005  03:47 AM            30,982 RaidTool_V10.sld
08/19/2005  04:32 PM           184,320 drvInterface.dll
08/12/2005  04:38 PM             5,226 ErrList.mlf
08/12/2005  04:38 PM         1,056,768 raid_tool.exe
09/21/2005  02:17 AM               627 VIA RAID TOOL.lnk

3. Import the driver component
(1) Copy all the files to a directory,
    e.g. "C:\VIADRIVERS\RaidTool_V552\".
(2) Create a directory, e.g. "D:\VIA_Repositories\", if there is
    none.
(3) Open Component Database Manager under Microsoft Windows
    Embedded Studio.
(4) Click on the "Repository" and then "Repository Roots..." buttons.
    Type in the complete path of the repositories directory,
    for example "D:\VIA_Repositories\". Click on the "Add" button
    and answer "Yes".
(5) Click on the "Database", "Import...", and then "..." buttons.
    Navigate to directory "C:\VIADRIVERS\RaidTool_V552\" and
    then choose the .SLD file. Next, pull down "Repository root"
    drop-down and select "D:\VIA_Repositories\". Click on the
    "Import" and then "Close" buttons to close the dialog.
(6) Close the "Component Database Manager".
(7) Add this component to target designer.